Dear team,
This may be a generic question but, could you show me whether if i.MX RT can support LCD display module which has non-rectangle shape such like round one?
I think every LCD panels which has non-rectangle shape have a resolution such like horizontal x vertical. And if the resolution and hardware I/F specs can meet, i.MX RT can support the LCD module. Correct?
Best Regards,
Miyamoto
Unfortunately, I.MXRT family LCD display can't support for the application.
Best regards
Hello Fangfang,
Do you mean that i.MX RT cannot support LCD display which has non-rectangle shape?
Could you show me why?
I think even such non-rectangle LCDs have resolution such like H x V. So I think if the spec are meet for requirement of i.MX RT, then i.MX RT can support such LCDs.
Best Regards,
Miyamoto
Hello,
May be it is not clear for previous reply. Sorry for it.
I.MXRT' output is standard RGB signal,
And we have not tested it on a round LCD. If the customer wants to use a round LCD,
we recommend that the customer does own project after the board is tested.
Hello fangfang,
OK. Now I understand that you did not test the round shaped LCDs.
Best Regards,
Miyamoto