Question, i.MX RT LCD Display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX RT LCD Display

2,037 Views
SLICE
Contributor IV

Dear team,

This may be a generic question but, could you show me whether if i.MX RT can support LCD display module which has non-rectangle shape such like round one?

I think every LCD panels which has non-rectangle shape have a resolution such like horizontal x vertical. And if the resolution and hardware I/F specs can meet, i.MX RT can support the LCD module. Correct?

Best Regards,

Miyamoto

Labels (4)
0 Kudos
Reply
5 Replies

1,918 Views
fangfang
NXP TechSupport
NXP TechSupport

Unfortunately, I.MXRT family LCD display can't support for the application.

Best regards

0 Kudos
Reply

1,918 Views
SLICE
Contributor IV

Hello Fangfang,

Do you mean that i.MX RT cannot support LCD display which has non-rectangle shape?

Could you show me why?

I think even such non-rectangle LCDs have resolution such like H x V. So I think if the spec are meet for requirement of i.MX RT, then i.MX RT can support such LCDs.

Best Regards,

Miyamoto

0 Kudos
Reply

1,918 Views
SLICE
Contributor IV

Hello fangfang‌,

I am still wait for your reply.

Best Regards,

Miyamoto

0 Kudos
Reply

1,918 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

May be it is not clear for previous reply. Sorry for it.

I.MXRT' output is standard RGB signal,
And we have not tested it on a round LCD. If the customer wants to use a round LCD,
we recommend that the customer does own project after the board is tested.

0 Kudos
Reply

1,918 Views
SLICE
Contributor IV

Hello fangfang‌,

OK. Now I understand that you did not test the round shaped LCDs.

Best Regards,

Miyamoto

0 Kudos
Reply