QuadSpi as general purpose "parallel" SPI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QuadSpi as general purpose "parallel" SPI?

894件の閲覧回数
mountainee
Contributor I

I am currently evaluating the i.MX RT1064 and its RT10xx cousins.

I have 4 identical high bandwidth SPI peripherals that I need to control in identical ways (analogous to SIMD), but I need a separate MOSI and MOSI line per each of the four peripheral.  I therefore need 9 lines: 1-CLK, 4-MOSI, 4-MISO with a MISO/MOSI pairs for each peripheral (see attached simple schematic).  Is it possible to map Quad SPI back to a dumb full-duplex mode?  I'm looking to just DMA block of data into memory. 

ラベル(4)
0 件の賞賛
返信
1 返信

813件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Is it possible to map Quad SPI back to a dumb full-duplex mode?
-- Actually, I'm not very clear with this question, whether you can explain it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信