PWM not working without XBAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM not working without XBAR

1,051 Views
shaileshnsec
Contributor II
Hi,
 
We are trying to generate the PWM signals in imxrt 1050 EVKE evaluation board, not using the QTMR module.
In the example code, XBAR is used for generating signals, if we don't use that, not able to see the signals generated. Checking the signals using logic analyzer.
 
Can you please suggest me how to disable XBAR and generate PWM signals?
 
Thanks /Shailesh
0 Kudos
Reply
2 Replies

1,022 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Shailesh,

There is not a way to generate the PWM without the XBAR.

I see that you already asked a bit more about this setup on the following thread, so I’m adding it in case another user finds it helpful.

https://community.nxp.com/t5/i-MX-RT/Issue-in-generating-PWM-signal-without-xbar-input/m-p/1288033

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply

1,014 Views
shaileshnsec
Contributor II

Thanks Gustavo.

0 Kudos
Reply