Not able to Flash on i.MRT1176 .Failed on connect: Ee(42). Could not connect to core. No connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to Flash on i.MRT1176 .Failed on connect: Ee(42). Could not connect to core. No connection

1,611件の閲覧回数
Ankarao_Ittadi
Contributor I

Hi

When we are debugging RT1176, we are facing followinng issue.

Any body Please help us.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,605件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I'd like to know what exactly board you used.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,604件の閲覧回数
Ankarao_Ittadi
Contributor I

Hi we are Using Embedded  Artists i.MX RT1176 Developers kit (Rev PB2) Board.

 

You can find the more details on this link also.

 

https://www.embeddedartists.com/products/imx-rt1176-ucom/

#i.MX RT1176 EA(Embedded Artists)

0 件の賞賛
返信

1,597件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @Ankarao_Ittadi ,
Thanks for your reply.
Maybe you can try the below trick to recover.
1) Set the boot mode pins to Serial Downloader.
2) Power on the board, debug the demo project.
3) After that, power off and recover the boot mode pins to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信