Hello
I am using mimxrt117x evk kit with wifi test example(sdio) from sdk 12.0 .while using in debugging mode i am getting Closed Telnet Session msg randomly then debugging sessions closed completely.
Can you guide me why i am getting this error??
Hello,
Could you please also help us with the module you are using with the example ? Also , could you please also help me confirm that you are using UART and not semihosting ? Also which version of the MCUXPresso IDE are you using ? Did you made some modification to the code example ?
Regards
Hello thanks for Reply
my problem is solved
Are you using MCUXpresso IDE project?The default build is Xip Build, the stability may be affected by flashloader, you can switch to RAM build as below: