MIMXRT1060-EVKB LPSPI testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060-EVKB LPSPI testing

Jump to solution
1,245 Views
niz
Contributor III

I am trying test the LP SPI on the MIMXRT1060-EVKB Board, and I found that one of the SPI port is on the J17 connector, from the schematic there are DNP commented on the SPI lines.  

niz_1-1657299901846.png

Does that mean that I need to short R356, R350, R346 and R362 to make it work with the connector J17? 

 

Thanks a lot for your help 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,214 Views
niz
Contributor III

Hi Omar 

Thanks for the confirmation, that is helpful. 

I have one more question about the CAN testing: 

According to the circuit, it needs the 10K pull up resister: 

niz_0-1657825980139.png

So is it OK that we just short the R269 and put the CAN_STBY to high by the MCU without putting 10K resister at R268? 

I did this modification without connecting R268, drive the CAN_STBY to high by MCU. 

And I cannot send CAN out successfully by running "flexcan_ping_pong_buffer_transfer" example. The MbStatusFlags are always 0 (IFLAG1 and IFLAG2).

So is pull up resister R 267 is a must? or something else might be wrong? 

 

Thanks a lot for your help 

 

Ni  

 

 

View solution in original post

0 Kudos
Reply
3 Replies
1,225 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
You are correct, the connections need to be shorted to use those pins.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply
1,215 Views
niz
Contributor III

Hi Omar 

Thanks for the confirmation, that is helpful. 

I have one more question about the CAN testing: 

According to the circuit, it needs the 10K pull up resister: 

niz_0-1657825980139.png

So is it OK that we just short the R269 and put the CAN_STBY to high by the MCU without putting 10K resister at R268? 

I did this modification without connecting R268, drive the CAN_STBY to high by MCU. 

And I cannot send CAN out successfully by running "flexcan_ping_pong_buffer_transfer" example. The MbStatusFlags are always 0 (IFLAG1 and IFLAG2).

So is pull up resister R 267 is a must? or something else might be wrong? 

 

Thanks a lot for your help 

 

Ni  

 

 

0 Kudos
Reply
1,212 Views
niz
Contributor III

Never mind, I just figure that out, I need to put the standby to low instead of high. 

Now I can see it is transmitting messages. 

Thanks 

 

Ni 

0 Kudos
Reply