M.2 modules with BT passthrough

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M.2 modules with BT passthrough

Jump to solution
1,373 Views
romitchatterjee
Contributor V

Which M.2 modules have BT-passthrough functionality implemented in it? I am using an NXP i.MX RT 1060 EVK.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,281 Views
puja_sah
Contributor II

Hello Romit,

The new SDK 2.6.2 for i. MX RT 1060 EVK includes the BT-passthrough functionality for 1DX EVB. Currently, it is implemented in 1DX only but 1LV and 1MW are on the roadmap to have BT-passthrough functionality implemented on them.

You can download the SDK from Welcome | MCUXpresso SDK Builder 

For more information about the module, please refer to https://wireless.murata.com/type-1dx.html 

Also, you can find the quick start guide for i. MX RT here https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf 

Hope it helps.

Thanks,

Puja

View solution in original post

0 Kudos
Reply
2 Replies
865 Views
kevin512
Contributor I

Is 1MW BT passthough supported on latest SDK?

0 Kudos
Reply
1,282 Views
puja_sah
Contributor II

Hello Romit,

The new SDK 2.6.2 for i. MX RT 1060 EVK includes the BT-passthrough functionality for 1DX EVB. Currently, it is implemented in 1DX only but 1LV and 1MW are on the roadmap to have BT-passthrough functionality implemented on them.

You can download the SDK from Welcome | MCUXpresso SDK Builder 

For more information about the module, please refer to https://wireless.murata.com/type-1dx.html 

Also, you can find the quick start guide for i. MX RT here https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf 

Hope it helps.

Thanks,

Puja

0 Kudos
Reply