Linux MTD flexSPI driver for IMXRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux MTD flexSPI driver for IMXRT1050

1,267 Views
vinaymanikkoth
Contributor II

Hi,

from where i can get a linux MTD flexSPI driver for imxrt1050 MCU? i am using IMXRT1050-EVKB kit from nxp. 

Thanks

Vinay

Labels (1)
0 Kudos
Reply
2 Replies

1,039 Views
art
NXP Employee
NXP Employee

Since there is no Linux port for the i.MX RT series processors, no FlexSPI MTD driver is available for them.

The bare metal and FreeRTOS FlexSPI memory drivers are available as the part of the MCUXpresso SDK for i.MX RT series processors:

https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-t...


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,039 Views
ali_karademir
Contributor I

Where can I find FreeRTOS FlexSPI driver? It does not seem to be part of most recent SDK of imxrt1050. 

0 Kudos
Reply