LVGL 8 and VGLite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVGL 8 and VGLite

989件の閲覧回数
masterboy
Contributor III

Hi,

I am working on a project that uses the LVGL graphics library (8.3.8). I am using an iMX RT1060 processor as GPU. The NXP SDK I used to bring the LVGL graphics library to life uses PXP for acceleration. The LVGL library also supports VGLite acceleration. I searched the SDK for an example use case, but didn't find one. Could I get the code to use LVGL with VGLite acceleration?
Dale I wonder how much different is PXP vs VGLite? Which is more powerful?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

976件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @masterboy,

You can find code that implements VGLite acceleration bundled with Application Notes. Namely, AN13075 (and the associated AN13075SW) and AN13778 (and the associated AN13778SW).

BR,
Edwin.

0 件の賞賛
返信

934件の閲覧回数
masterboy
Contributor III

I'm sorry, but I didn't specify the processor I'm using in the project. It is an iMX RT 1060/1062. Does this processor support VGLite?

0 件の賞賛
返信

926件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @masterboy,

Thanks for clarifying. I'm afraid the RT1060 does not support it. Sorry for the inconvenience this may cause.

BR,
Edwin.

0 件の賞賛
返信