Is there a function like DAC output on i.MX RT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a function like DAC output on i.MX RT1060

ソリューションへジャンプ
1,025件の閲覧回数
kenji
Contributor IV

Hi All

I'm working on BLDC motor control, with MIMXRT1060-EVK.

For debug, to visualize the motor control calculation result, I would like to output via DAC.

However i.MX RT 1062 device has no DAC function to output outside of the device.
Reading the user manual, it seem that only can output inside of the device.

I tried to visualize with SWO and FreeMASTER, but for sampling frequency problem, I could not use it. Both tools sampling freq are too slow to use.

Is there any tricks to output DAC, outside of the device?

Or is there a way to output the internal calculation result at high speed? The control cycle of the motor is 50kHz.

タグ(2)
0 件の賞賛
返信
1 解決策
1,015件の閲覧回数
mjbcswitzerland
Specialist V

Hi

PWM + low pass filter (eg. simple R/C filter) = DAC

Regards

Mark

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,016件の閲覧回数
mjbcswitzerland
Specialist V

Hi

PWM + low pass filter (eg. simple R/C filter) = DAC

Regards

Mark

 

0 件の賞賛
返信
995件の閲覧回数
kenji
Contributor IV

Hi @mjbcswitzerland -san

Yes, I know.
Maybe that's the only way for MIMXRT1060-EVK, so I'll use a filter.

Thank you!

0 件の賞賛
返信