Is there a function like DAC output on i.MX RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a function like DAC output on i.MX RT1060

Jump to solution
924 Views
kenji
Contributor IV

Hi All

I'm working on BLDC motor control, with MIMXRT1060-EVK.

For debug, to visualize the motor control calculation result, I would like to output via DAC.

However i.MX RT 1062 device has no DAC function to output outside of the device.
Reading the user manual, it seem that only can output inside of the device.

I tried to visualize with SWO and FreeMASTER, but for sampling frequency problem, I could not use it. Both tools sampling freq are too slow to use.

Is there any tricks to output DAC, outside of the device?

Or is there a way to output the internal calculation result at high speed? The control cycle of the motor is 50kHz.

Tags (2)
0 Kudos
Reply
1 Solution
914 Views
mjbcswitzerland
Specialist V

Hi

PWM + low pass filter (eg. simple R/C filter) = DAC

Regards

Mark

 

View solution in original post

0 Kudos
Reply
2 Replies
915 Views
mjbcswitzerland
Specialist V

Hi

PWM + low pass filter (eg. simple R/C filter) = DAC

Regards

Mark

 

0 Kudos
Reply
894 Views
kenji
Contributor IV

Hi @mjbcswitzerland -san

Yes, I know.
Maybe that's the only way for MIMXRT1060-EVK, so I'll use a filter.

Thank you!

0 Kudos
Reply