IMXRT1170 Gui Guider project VS MCUXpresso lvgl project performances

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1170 Gui Guider project VS MCUXpresso lvgl project performances

Jump to solution
751 Views
ahmedhrabi
Contributor III

Hi all, 

I'am using Gui Guider to draw a little lvgl list on imxrt1176 evk. And when launching the simulation on the EVK through the Gui Guider the list works as charm, however when i generate the same example, through Gui Guider, to an MCUXpresso project, build it, and flash it with MCUXpresso on the EVK, the list usage (scroll click..) became too slow ! Any explications ? 

(I can attach the project if needed)

Regards,

HRABI.

0 Kudos
Reply
1 Solution
721 Views
ahmedhrabi
Contributor III

Hello Carlos,

Well i found that with release compilation i don't have the problem. So with debug compilation the application is slower.

Regards.

View solution in original post

0 Kudos
Reply
2 Replies
722 Views
ahmedhrabi
Contributor III

Hello Carlos,

Well i found that with release compilation i don't have the problem. So with debug compilation the application is slower.

Regards.

0 Kudos
Reply
732 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

We don't have issue about it, so, could you provide more details about this?