We are using the custom board with MIMXRT1011CAE4A Processor .In this we are able to run the example code (evkmimxrt1010 flexspi_nor_polling_transfer)from RAM in MCU Xpresso IDE.But the issue is we are unable to run the code from FLASH,it shows this error "0xdeadbeee" .and below are the MCU config settings related to flash.
Hi @syed1 ,
Thanks for your interest in NXP MIMXRT series!
For execution in external flash, I don't see a flash driver from your screenshot. We need to configure the corresponding flash driver file. Also, please check the following two macros:
Best regards,
Gavin
Hello Gavin_Jia
Does this controller have internal flash, if it is available how to load my code into internal flash of the controller (MIMXRT1101CAE4A).
Right now, we are running our code in the internal RAM, but we want to run the code in flash so that even after power reset the code will exist in the flash.
Hi @syed1 ,
There is not a internal flash inside RT1010. Using XIP-capable external flash can also accomplish your goals. Could you provide more information for me? What is the part number of your flash and how does it communicate with the chip? From which port? This part is best chosen to be consistent with EVK so that no other changes will be needed. And could you verify the code with EVK first if possible?
Looking forward for your input.
Best regards,
Gavin
Hi Gavin,
Thanks for reaching out. Sure, I can provide more information on the external flash for RT1010.
For the external flash, we're using the Micron nor flash series, specifically the MT25QU512ABB. This flash chip communicates with the RT1010 microcontroller through the Quad-SPI (QSPI) interface at port A.
Currently, we are using evkmimxrt1010_nor_polling_transfer sdk example. We have already debugged this code in MCU expresso ide, and it runs for it (in ram).
How can we dump this code in external flash so that booting happens from there?
Best regards, Syed
Hello Gavin_Jia
We have executed the code after adding flash driver file in MCU settings, but still getting the same error. Also checked the macros that you've mentioned.