IMXRT 1052 Storage Temperature Range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT 1052 Storage Temperature Range

ソリューションへジャンプ
730件の閲覧回数
omerkaanbasakin
Contributor IV

Hello,

We are using i.MX RT1052. As far as we can see in the datasheet, the minimum storage temperature is -40°C. Has the test been done at -55°C? Is there information that can be given for -55°C?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
713件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
714件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 件の賞賛
返信