Hello,
We are using i.MX RT1052. As far as we can see in the datasheet, the minimum storage temperature is -40°C. Has the test been done at -55°C? Is there information that can be given for -55°C?
Thanks in advance.
已解决! 转到解答。
Hi,
As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.
Sorry for the inconvenience.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------
Hi,
As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.
Sorry for the inconvenience.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------