I2C master polling error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C master polling error

1,674 次查看
mtuxpe
Contributor III

Hello community,

I am trying to connect I2C light sensor (polling) to i.MX RT1010 EVK using MCUXpresso IDE

The sensor  TSL2561 I2C slave is connect to J57. I just want to detect the sensor by reading register TSL2561_REGISTER_ID = 0xa.

J57

GND = pin 14

3.3V = pin 16

i2C1_SDA = pin 18

i2C1_SCL = pin 20

status_t result;

BOARD_ConfigMPU();
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();

/*Clock setting for LPI2C*/
CLOCK_SetMux(kCLOCK_Lpi2cMux, LPI2C_CLOCK_SOURCE_SELECT);
CLOCK_SetDiv(kCLOCK_Lpi2cDiv, LPI2C_CLOCK_SOURCE_DIVIDER);

LPI2C_MasterGetDefaultConfig(&masterConfig);

/* Change the default baudrate configuration */
masterConfig.baudRate_Hz = LPI2C_BAUDRATE;

/* Initialize the LPI2C master peripheral */
LPI2C_MasterInit(EXAMPLE_I2C_MASTER, &masterConfig, LPI2C_MASTER_CLOCK_FREQUENCY);

/* Initialize sensor devices */

g_master_txBuff[0] = TSL2561_REGISTER_ID;

result = wrI2Cdata();

if (result != kStatus_Success)
     printf("\r\nI2C device initialize failed! %d\r\n",result);

result = rdI2Cdata();

if (result != kStatus_Success)
     printf("\r\nI2C device initialize failed! %d\r\n",result);

status_t wrI2Cdata (void) {

status_t reval;
size_t txCount = 0x1;

reval = LPI2C_MasterStart(EXAMPLE_I2C_MASTER, g_sensor_address[0], kLPI2C_Write);
if (kStatus_Success == reval) {

    LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
    while (txCount){
        LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
    }
/* Check communicate with slave successful or not */
    while (LPI2C_MasterGetStatusFlags(EXAMPLE_I2C_MASTER) & kLPI2C_MasterNackDetectFlag){
    }

    reval = LPI2C_MasterSend(EXAMPLE_I2C_MASTER,g_master_txBuff , 1);

    if (reval != kStatus_Success)
        return reval;

   reval = LPI2C_MasterStop(EXAMPLE_I2C_MASTER);

}

   return reval;
}

status_t rdI2Cdata (void)
{
status_t reval;
size_t txCount = 0x1;

reval = LPI2C_MasterStart(EXAMPLE_I2C_MASTER, g_sensor_address[0], kLPI2C_Read);
if (kStatus_Success == reval) {

    LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
    while (txCount)
    {
        LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
    }
/* Check communicate with slave successful or not */
    while (LPI2C_MasterGetStatusFlags(EXAMPLE_I2C_MASTER) & kLPI2C_MasterNackDetectFlag)
    {
    }

    reval = LPI2C_MasterReceive(EXAMPLE_I2C_MASTER, g_master_rxBuff, 1);
    if (reval != kStatus_Success)
    {
        return reval;
    }

    reval = LPI2C_MasterStop(EXAMPLE_I2C_MASTER);

}

return reval;
}


I2C device initialize failed! 909

I2C device initialize failed! 909

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,494 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Marcio, 

I'm not familiar with the sensor you are using, however, I recommend you using the example polling_b2b_master from the SDK, this example works properly. I would also recommend you to check that the configurations you are using for the Master are supported by your sensor, for example, you can verify that the baudrate that you are setting on the Master is not too fast for your sensor. 

Best regards, 

Victor 

0 项奖励
回复