I2C Master reports Bus Busy when SDA/SCL are high

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C Master reports Bus Busy when SDA/SCL are high

752件の閲覧回数
jamesk
Contributor III

I understand there is a workaround available for this issue here, https://community.nxp.com/t5/i-MX-Processors/Master-I2C-Bus-Busy/m-p/1202554

But it would be great if someone(NXP) could provide some explanation as to why the driver(LPI2C_MasterGetStatusFlags()) returns "bus busy" when both SDA/SCL are high.

I also see this often enough on our dev. product which is built on using NXP iMXRT 1052.

Shouldn't this be considered as a NXP driver bug?

0 件の賞賛
返信
0 返答(返信)