I'm running the evkmimxrt1060_ota_mcuboot_client_enet example with the default SBL from the evkmimxrt1060_mcuboot_opensource example on the EVA board using MCUXpresso version 11.10.0. I followed the readme files for both examples but encountered an issue where the bootloader treated the signed binary as faulty.
The serial log shows the following:
hello sbl.
Disabling flash remapping function
Bootloader Version 1.10.0
Primary slot: version=1.0.0+0
Image 0 Secondary slot: Image not found
Erasing faulty image in the primary slot.
after further investigation, I found in the "boot_select_or_erase" function
if (active_swap_state->magic != BOOT_MAGIC_GOOD ||
(active_swap_state->copy_done == BOOT_FLAG_SET &&
active_swap_state->image_ok != BOOT_FLAG_SET)) {
//print status
BOOT_LOG_INF("magic: 0x%lx, copy_done: 0x%lx, image_ok: 0x%lx",
(unsigned long)active_swap_state->magic,
(unsigned long)active_swap_state->copy_done,
(unsigned long)active_swap_state->image_ok);
/*
* A reboot happened without the image being confirmed at
* runtime or its trailer is corrupted/invalid. Erase the image
* to prevent it from being selected again on the next reboot.
*/
BOOT_LOG_DBG("Erasing faulty image in the %s slot.",
(active_slot == BOOT_PRIMARY_SLOT) ? "primary" : "secondary");
rc = flash_area_erase(fap, 0, flash_area_get_size(fap));
assert(rc == 0);
flash_area_close(fap);
rc = -1;
}
"state" was read to
magic: 0x3, copy_done: 0x3, image_ok: 0x3
I'm using the imgtool and the private key provided with the SDK. Here's my script for signing the binary:
python3 ../sign_tool/imgtool.py sign \
--key ../sign_tool/sign-rsa2048-priv.pem \
--align 4 \
--header-size 0x0400 \
--pad-header \
--slot-size 0x200000 \
--max-sectors 800 \
--version "1.0" \
binaries/evkmimxrt1060_ota_mcuboot_client_enet.bin \
binaries/app_binary_SIGNED.bin
Any idea what might be going wrong?