How to use JTRACE on RT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use JTRACE on RT1064

990 次查看
MrHWT
Contributor I

How to use JTRACE on RT1064?Thank you.

0 项奖励
回复
7 回复数

914 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @MrHWT ,

Thanks for the interest in NXP MIMXRT series!

 

Regarding to the EVK, to connect an external JTAG debugger first you need to remove jumpers J47, J48, and J49. Then you should use connector J21 to connect your external debug probe to the RT.

For your customer board, please refer to the EVK hardware design. And just as a heads up, the debug interface of the RT10xx comes by default to work with SWD, if you want to communicate with JTAG, you will need to burn the fuse DAP_SJC_SWD_SEL.

Best regards,

Gavin

0 项奖励
回复

903 次查看
MrHWT
Contributor I

Thank you for your reply。How to configure the project to use TRACE?

0 项奖励
回复

862 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @MrHWT ,

There is a detailed Application Note on this topic:
https://www.nxp.com/docs/en/application-note/AN12877.pdf

Hope it helps!

 

Best regards,
Gavin

0 项奖励
回复

938 次查看
Masmiseim
Senior Contributor I

As you are using J-Trace. Did you tried the example from Segger?

https://wiki.segger.com/Tracing_on_NXP_iMX_RT1050_(iMX_RT1050_Trace_Reference_Board)

This is for 1050, but the 1064 should work the same way.

0 项奖励
回复

742 次查看
MrHWT
Contributor I

Same board. RT1052 is ok,  RT1064 can not trace. All use the example code from the official website.

https://wiki.segger.com/Tracing_on_NXP_iMX_RT1050_(iMX_RT1050_Trace_Reference_Board)

https://wiki.segger.com/i.MXRT1060#Tracing_on_NXP_iMXRT1064

 

0 项奖励
回复

979 次查看
Masmiseim
Senior Contributor I

I guess you are using the Evaluation Board, right?

It is not possible to use the trace functionality with this board as the Trace-Pins are not connected to the JTAG-Connector.

0 项奖励
回复

945 次查看
MrHWT
Contributor I
No, I used my own board and led out the pins
0 项奖励
回复