How to configure for GD25Q40C using MCUBootUtility software?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure for GD25Q40C using MCUBootUtility software?

701件の閲覧回数
wqazoplm
Contributor I

Hi All,

How to configure for GD25Q40C using MCUBootUtility software?

Device_Configration.jpg

Looking forward to your answer!

Best regards!

0 件の賞賛
返信
1 返信

656件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

There is an option called [Use Typical Device Model] on the page. The NXP-MCUBootUtility pre-defines some commonly used Multi-IO SPI NOR Flash model models, if the external storage chip on the development board happens to be in pre-defined model list, you can select the corresponding model directly in the [Use Typical Device Model] without having to configure it one by one in the Nor Option.

If you do not see the option for the same part number under typical devices. Then you must select "no" for typical devices, next you must choose the parameters related to what you will be using and this will generate a generic device.

Could you please attempt this?

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信