How to configure for GD25Q40C using MCUBootUtility software?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure for GD25Q40C using MCUBootUtility software?

704 次查看
wqazoplm
Contributor I

Hi All,

How to configure for GD25Q40C using MCUBootUtility software?

Device_Configration.jpg

Looking forward to your answer!

Best regards!

0 项奖励
回复
1 回复

659 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

There is an option called [Use Typical Device Model] on the page. The NXP-MCUBootUtility pre-defines some commonly used Multi-IO SPI NOR Flash model models, if the external storage chip on the development board happens to be in pre-defined model list, you can select the corresponding model directly in the [Use Typical Device Model] without having to configure it one by one in the Nor Option.

If you do not see the option for the same part number under typical devices. Then you must select "no" for typical devices, next you must choose the parameters related to what you will be using and this will generate a generic device.

Could you please attempt this?

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复