Hello everyone, i meet a emergence issue in our design. please, find someone to resolve this problem.
Look at 1050 user guide section SEMC controller, below the picture:
the MCR register bit[6] can change NOR/PSRAM RDY# polarity, BUT i can not find how to configure WAIT/RDY# pin. Because follow the IOCR register no bit to configure this function. That is very confused and mislead our design. Have someone can help me, thx.
Hi 钱汉望 钱 ,
Please check this table in chapter 24.4.3 Pin Mux in SEMC:
So, I think you can configure IOCR.MUX_RDY to 111, it is PSRAM address bit 27.
Wish it helps you!
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Think you for your reply, i can configure IOCR.MUX_RDY to bit:111, But we need BUSY#/WAIT# pin as input function for slave device indicate ready for WE/RD data in sram bus. So, how to configure BUSY/WAIT pin just like NAND device ready/wait input?
Hi 钱汉望 钱.
Which SRAM you are using?
Can you share your partial schematic about your SRAM with RT1052?
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------