FlexIO parallel input with external clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexIO parallel input with external clock

3,035件の閲覧回数
nimish1
Contributor I

I need to work with an 8 bit parallel ADC that emits a sampling clock up to 44MHz. Is it possible to configure the FlexIO to work off an external clock? Is there a sample available?

It'd be analogous to ST's PSSI/DCMI or even just a parallel camera module input with ext pixel clock.

0 件の賞賛
返信
2 返答(返信)

2,997件の閲覧回数
nimish1
Contributor I

Best I've found is hijacking code for streaming in camera data or this https://forum.pjrc.com/threads/66201-Teensy-4-1-How-to-start-using-FlexIO

NXP please make an easy flexio library! I don't want to be configuring shift registers!

 

0 件の賞賛
返信

3,026件の閲覧回数
Vyssotski
Contributor I

It is probably possible to get some piece of data from ADC by configuring flexSPI to use DQS pad as an input clock for data reading. After this one can perform Read data command similar to flash/RAM reading. However, you are probably interested in continuous non-stop ADC polling. Whether it is possible to have one read command to read infinite amount of data I don't know. Please post the answer when it is found.

0 件の賞賛
返信