Failed to debug MIMXRT1020

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to debug MIMXRT1020

ソリューションへジャンプ
497件の閲覧回数
ffjunq
Contributor I

Hello everybody.

My problem is to debug the MMIMXRT1020-EVK board
The problem started after I changed the value of an sdk project variable evkmimxrt1020_flexspi_nor_polling_transfer. In the flexspi_nor_enable_quad_mode() function I changed the value of the uint32_t writeValue variable. After that, I was never able to debug the board again. The following error appears:

ffjunq_0-1685475464444.png

I performed some tests to try to fix it, such as using a PE-Micro to write the firmware with the correct value of the writeValue variable, however, all operations return an invalid status.

Can anyone help me?

ラベル(1)
0 件の賞賛
返信
1 解決策
475件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ffjunq ,

  Please don't worry, you may download the code to the flash, and you may disable the quad mode, then it will cause the chip read the flash code in quad mode failed, then the boot failed, and you meet the issues.

   Now, please do the mass erase first, you can refer to this post:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...

If you still have issues about it, please kindly let me know.

Best Regards,

Kerry

元の投稿で解決策を見る

1 返信
476件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ffjunq ,

  Please don't worry, you may download the code to the flash, and you may disable the quad mode, then it will cause the chip read the flash code in quad mode failed, then the boot failed, and you meet the issues.

   Now, please do the mass erase first, you can refer to this post:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...

If you still have issues about it, please kindly let me know.

Best Regards,

Kerry