Ethernet CRS and JTAG TDO pin conflict in i.MXRT1062CVL5A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet CRS and JTAG TDO pin conflict in i.MXRT1062CVL5A

Jump to solution
2,890 Views
sumant_s_khalat
Contributor II

Is there any way to get around pin mapping conflict for Ethernet CRS and JTAG TDO in i.MXRT1062CVL5A. Both the pins don't support multiplexing. I have attached a screenshot for reference.

Labels (1)
Tags (2)
1 Solution
2,763 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sumant Khalate

Thanks for your reply.
The i.MX RT1062 supports the SWD interface.

pastedImage_2.png
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
2,763 Views
sumant_s_khalat
Contributor II

Thanks, jeremyzhou, another question on the same lines. Is there any other interface apart from JTAG that I can use to program i.MX RT1062? because I haven't seen SWD on it.

Have a great day,

Sumant

0 Kudos
Reply
2,764 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sumant Khalate

Thanks for your reply.
The i.MX RT1062 supports the SWD interface.

pastedImage_2.png
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,763 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sumant Khalate

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'm afraid the GPIO_AD_B0_10 is unable to work as JTAG TDO and ENET_CRS pins simultaneously.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------