EFUSE AREA WRITE OPERATIONS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EFUSE AREA WRITE OPERATIONS

ソリューションへジャンプ
557件の閲覧回数
SpeedyGonzaless
Contributor I

Hello,

I am using I.MX RT1170. I want to make the M4 processor the primary processor. There is a register in the EFUSE region for this.But i am wondering something. Can the change made in the Efuse region be undone? After M4 is selected, can M7 processor be primary again in different projects?

0 件の賞賛
返信
1 解決策
529件の閲覧回数
ramprakash09
Contributor II

Hi,

It look like that the primary processor is determined by a register in the EFUSE region. Once a change is made in the EFUSE region, it is typically permanent and cannot be undone. This is because the EFUSE region is usually used for one-time programmable (OTP) memory, which can only be written to once.

So, if you make the M4 the primary processor by changing the register in the EFUSE region, you will not be able to make the M7 the primary processor again in different projects. This is a critical decision and should be made with care.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
530件の閲覧回数
ramprakash09
Contributor II

Hi,

It look like that the primary processor is determined by a register in the EFUSE region. Once a change is made in the EFUSE region, it is typically permanent and cannot be undone. This is because the EFUSE region is usually used for one-time programmable (OTP) memory, which can only be written to once.

So, if you make the M4 the primary processor by changing the register in the EFUSE region, you will not be able to make the M7 the primary processor again in different projects. This is a critical decision and should be made with care.

Regards

0 件の賞賛
返信
525件の閲覧回数
SpeedyGonzaless
Contributor I

Hello,

Thank you for your support.

0 件の賞賛
返信