ECC check and inline encryption engine for SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC check and inline encryption engine for SDRAM

Jump to solution
1,720 Views
Nagaveni
Contributor II

Hi,

 We are using IMXRT1170 EVK , could you please share and guide how to do ECC check for SDRAM and Inline encryption engine enabling to read and write data to  SDRAM.

Thanks in advance,

1 Solution
1,707 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You can check this application note as well as this blog, although it is in Chinese it can be translated and contains helpful information:
-i.MX RT1170 ECC Application (nxp.com)
-痞子衡嵌入式:简析i.MXRT1170 XECC功能特点及其保护串行NOR Flash和SDRAM之道 - 痞子衡 - 博客园 (cnblogs.com)

Additionally, you might check the SDK examples as a reference for ECC and IEE.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,708 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You can check this application note as well as this blog, although it is in Chinese it can be translated and contains helpful information:
-i.MX RT1170 ECC Application (nxp.com)
-痞子衡嵌入式:简析i.MXRT1170 XECC功能特点及其保护串行NOR Flash和SDRAM之道 - 痞子衡 - 博客园 (cnblogs.com)

Additionally, you might check the SDK examples as a reference for ECC and IEE.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply