Drived SRAM by SEMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drived SRAM by SEMC

1,651件の閲覧回数
1668834026
Contributor I

Hello,

我使用RT1052驱动外部SRAM碰到一个很奇怪的现象。

我参照SDRAM的例程修改。。现在是,16字节的方式读写数据(一次读写4096字节,就是基于SDRAM的例程改的)的时候第一次执行不成功(没写入),而第二次执行才成功(而且还需要两次完整的读写操作才能写入,第一次读写和第二次读写加入延时,现象也一样),8位操作现象类似,我关闭DCache后两次执行都不成功(数据没写入)。

pastedImage_1.png

这是我SRAM的配置,更奇怪的是,我将时间参数配置部分全部写0,现象是一样的。请问这是什么原因?

status_t BOARD_InitSEMC(void)
{
semc_config_t config;
semc_sram_config_t sramconfig;
uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

/* Initializes the MAC configure structure to zero. */
memset(&config, 0, sizeof(semc_config_t));
memset(&sramconfig, 0, sizeof(semc_sram_config_t));

/* Initialize SEMC. */
SEMC_GetDefaultConfig(&config);
// config.dqsMode = kSEMC_Loopbackdqspad; /* For more accurate timing. */
SEMC_Init(SEMC, &config);

/* Configure SRAM. */
sramconfig.cePinMux = kSEMC_MUXCSX0;
sramconfig.addr27 = kSEMC_MORA27_NONE;
sramconfig.address = EXAMPLE_SEMC_START_ADDRESS;
sramconfig.memsize_kbytes = 128 * 1024; /* 128MB = 128*1024*1KBytes*/;
sramconfig.addrPortWidth = 16;
sramconfig.advActivePolarity = kSEMC_AdvActivehigh;
sramconfig.addrMode = kSEMC_AddrDataMux;
sramconfig.burstLen = kSEMC_Nor_BurstLen1;
sramconfig.portSize = kSEMC_PortSize16Bit;
sramconfig.tCeSetup_Ns = 7;
sramconfig.tCeHold_Ns = 7;
sramconfig.tCeInterval_Ns = 15;
sramconfig.tAddrSetup_Ns = 5;
sramconfig.tAddrHold_Ns = 2;
sramconfig.tWeLow_Ns = 20;
sramconfig.tWeHigh_Ns = 0;
sramconfig.tReLow_Ns = 20;
sramconfig.tReHigh_Ns = 7;
sramconfig.tTurnAround_Ns= 8;
sramconfig.tAddr2WriteHold_Ns = 10;
sramconfig.tWriteSetup_Ns = 0;
sramconfig.tWriteHold_Ns = 0;
sramconfig.latencyCount = 0;
sramconfig.readCycle = 0;

return SEMC_ConfigureSRAM(SEMC, &sramconfig, clockFrq);
}

原理图部分:

MCU

pastedImage_2.png

SRAM

pastedImage_3.png

另外,还有个问题:

我在RT1052手册中看到有一段描述,这个区域分配是代表地址分配范围吗?如果是,每个区域对应的地址是什么?

pastedImage_4.png

现在我给SRAM的地址是0x8000 0000。

期待你的解答。

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,514件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi 植渲 周,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) For the first question, I think you need to use a logic analyzer or oscilloscope to adjust the configuration of SRAM config struct.
2) 这个区域分配是代表地址分配范围吗?如果是,每个区域对应的地址是什么?
-- Region 对应给个Base register, 在寄存器中可以配置对应设备的基地址。

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,514件の閲覧回数
1668834026
Contributor I

Hello, jeremyzhou,

关于第二个问题,我还有些疑问:

1.假如我挂载两片SRAM,这个地址我怎么分配,是按SRAM的大小来分吗,还有片选线怎么连接,因为我看见SRAM的片选线只有CS6,这么说SEMC不支持挂载多片SRAM是吗?

pastedImage_1.png

2.关于SDRAM的区域分配问题,下图可以看到SDRAM分为四个区域,地址区域和片选信号有什么联系,如果我没理解错的话,区域划分是自己填写的,假设我设置SDRAM1 ADDR = 0X8000 0000,SDRAM2 ADDR = 0X8001 0000,当我访问 0X8000 0000时SEMC会自动发送一个CS0信号选中SDRAM1,这样理解是否正确?

pastedImage_2.png

0 件の賞賛
返信

1,514件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi 植渲 周,

感谢回复。

1)假如我挂载两片SRAM,这个地址我怎么分配,是按SRAM的大小来分吗,还有片选线怎么连接,因为我看见SRAM的片选线只有CS6,这么说SEMC不支持挂载多片SRAM是吗?

-- 是的,不支持挂载多片SRAM。

2) 2.关于SDRAM的区域分配问题,下图可以看到SDRAM分为四个区域,地址区域和片选信号有什么联系,如果我没理解错的话,区域划分是自己填写的,假设我设置SDRAM1 ADDR = 0X8000 0000,SDRAM2 ADDR = 0X8001 0000,当我访问 0X8000 0000时SEMC会自动发送一个CS0信号选中SDRAM1,这样理解是否正确?

-- 是的,理解正确。

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信