We need RT1050 EVK LAY-29538_A2.brd file in ASCII (ALG) or already imported into Altium Designer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We need RT1050 EVK LAY-29538_A2.brd file in ASCII (ALG) or already imported into Altium Designer

3,327 Views
MehmetAliIpin
Contributor V

Dear Sir/Madam

Hello,

Since we use Altium, we need the ASCII(ALG) or already altium converted files of RT1050 EVK LAY-29538_A2.brd file.

I would appreciate if anybody have and send these files.

Thanks and best regards.

Mehmet Ali Ipin.

Labels (1)
13 Replies

2,846 Views
ffurkanyilmazz
Contributor II

Hello,

I have been facing the same problem for some quiet time. I am using Altium, can you also send the  corresponding files to me?

Regards,

Furkan.

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

ffurkanyilmazz@gmail.com 

Hello,

  Please create separate Community thread. 

Support | NXP 

Regards,

Yuri.

2,846 Views
ffurkanyilmazz
Contributor II

Dear Yuri,

I created a seperate thread for this (RT1050 Dev. board layout file (LAY-30168_A.brd) correspondant altium files are needed

Thank you,

Furkan

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

ffurkanyilmazz@gmail.com 

Hello,

    As I see the  request is answered.

(https://community.nxp.com/thread/532207 )

Regards,

Yuri.

2,846 Views
ffurkanyilmazz
Contributor II

Dear YuriMuhin_ng‌,

Yes it seem it was. Thank you,

Regards,

Furkan

0 Kudos
Reply

2,846 Views
MehmetAliIpin
Contributor V

Dear Yuri,

Thank you very much,

Best regads.

Mehmet.

0 Kudos
Reply

2,846 Views
mehmetipin
Contributor II

Dear Yuri,

I already requested service and we have NDA with NXP.

Thanks alot for your kind helps.

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

Hello,

  What is case number? 

Regards,

Yuri.

0 Kudos
Reply

2,846 Views
MehmetAliIpin
Contributor V

Hello,

NDA#78287

Best regards.

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I meant creation request under the following 

https://nxpcommunity.force.com/community/CommunityNXPCreateCase 

~Yuri.

2,846 Views
mehmetipin
Contributor II

Dear Yuri,

I have received design files including LAY-29538_A2.brd file in my disk, without a link. But I could not see a control button in this page to upload it.

May I send it to your mail address, or could you tell me how I can upload file?

 

Best regards.

Mehmet.

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In any case, I think it makes sense to use NXP service request, since the EVK files are not 
published yet on the Web. I will use my .BRD file.   

Regards,

Yuri.

0 Kudos
Reply

2,846 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please create request and provide Your LAY-29538_A2.brd file under request.

Support|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply