Does the MIMXRT1060-EVKB contain a camera?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the MIMXRT1060-EVKB contain a camera?

667 次查看
anonymous3957
Contributor I

EDIT: This is quite urgent for me! Please help me ASAP

According to the MIMXRT1060-EVKB Board User Manual, it contains:

- MIMXRT1060-EVKB board

- USB Type A to micro-B cable

- Camera, CA111C based on MT9M114

but looking at this unboxing, I just can't spot it. On the Packing List shown in the video, there are actually 3 components:

- 700-47858: PWA, MIMXRT1060-EVKB

- 600-77315: USB 2.0 TO MICRO 1.0M

- 926-79035: QSG, MIMXRT1060-EVKB

but I just see the Board and the USB cable in the video. So maybe one of two Product Numbers which isn't the USB cable is supposed to be the camera (even though I don't see it)? I can't find any information regarding those PNs on the internet.

0 项奖励
回复
1 回复

605 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @anonymous3957 ,

   About the RT board situation, you can find it from the website:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1060-eva...

kerryzhou_0-1659346399276.png

kerryzhou_1-1659346406700.png

 

I find the EVK contains the camera, but the EVKB didn't list it.

So, the MIMXRT1060-EVKB should don't have it.

If you still have questions about it, you can contact with the side where you buy the board, if it is distributor, check with distributor, if it is the NXP web, you can check with:

direct@nxp.com

 

Wish it helps you!

Best Regards,

kerry

 

0 项奖励
回复