DAC on MIMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,201件の閲覧回数
markus_winkhoef
Contributor II

Hello NXP Community,

does the RT1064 controller contains a DAC output with which i can provide an analog voltage to a Pin on the microcontroller?

Best regards,

Markus

0 件の賞賛
返信
1 解決策
1,116件の閲覧回数
mjbcswitzerland
Specialist V

Hi Markus

The RT1064 doesn't have a DAC for external use but DACs can be made with a PWM output and an RC filter, which may be a suitable solution for your case.

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

元の投稿で解決策を見る

1 返信
1,117件の閲覧回数
mjbcswitzerland
Specialist V

Hi Markus

The RT1064 doesn't have a DAC for external use but DACs can be made with a PWM output and an RC filter, which may be a suitable solution for your case.

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]