Can 'i.MX RT 1050/105' support both Alexa and Google Assistant ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can 'i.MX RT 1050/105' support both Alexa and Google Assistant ?

ソリューションへジャンプ
1,828件の閲覧回数
yu-chiangtsao
Contributor I

I hope to make a device which can support both Alexa Voice Services and google assistant ,and I saw your audio solutions as figure.

 Can I use i.MX RT 1050/1051 ? And do you have any recommendation about microphone position? How should we set the distance between microphones which is better in your algorithm?pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,514件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi,

in i.MX6ULL and i.MX7D a full Linux distribution is used, this makes it easy to set the audio services.

i.MXRT does not support a full Linux distribution, only uCLinux and FreeRTOS. It should be possible to add voice services but we don't have any support. Theoretically you will need to add all the support packages required by Alexa and then cross compile the Alexa platform for M7 and this means a huge effort.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,514件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Yu-Chiang Tsao,

I was informed that the NXP solutions team is currently working on an i-MX RT based solution for an Alexa and Google assistant, as this is a costumer driven process they are always looking for customer input. Consequently, if OK with you one of them will contact you shortly.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,515件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi,

in i.MX6ULL and i.MX7D a full Linux distribution is used, this makes it easy to set the audio services.

i.MXRT does not support a full Linux distribution, only uCLinux and FreeRTOS. It should be possible to add voice services but we don't have any support. Theoretically you will need to add all the support packages required by Alexa and then cross compile the Alexa platform for M7 and this means a huge effort.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信