Bring up of custom RT685 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bring up of custom RT685 board

2,107 Views
Hthornburgh
Contributor II

Hello,

I am trying to bring up our custom DSP board with the RT685. I am following this article here, https://community.nxp.com/t5/Blogs/i-MX-RT685-SuperMonkey-QSPI-Bring-up-with-MCUXpresso-and-Segger/b...

but am having issues flashing to the device. I am using a MCU-Link Debug Probe in CMSIS/DAP mode and get this issue when trying to flash a modified version of hello_world demo.

We are using a QSPI by Infineon pn: S25FL256SDPMFV001

I am getting an error that states: "Dynamic flash driver startup failed to provide flash parameters"

Here is what my boot header looks like

/*
 * Copyright 2020 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */
#include "flash_config.h"
#include "board.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.flash_config"
#endif

/*******************************************************************************
 * Code
 ******************************************************************************/
#if defined(BOOT_HEADER_ENABLE) && (BOOT_HEADER_ENABLE == 1)
#if defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".flash_conf")))
#elif defined(__ICCARM__)
#pragma location = ".flash_conf"
#endif

const flexspi_nor_config_t flexspi_config = {
    .memConfig =
        {
            .tag                 = FLASH_CONFIG_BLOCK_TAG,
            .version             = FLASH_CONFIG_BLOCK_VERSION,
            .csHoldTime          = 3,
            .csSetupTime         = 3,

            .waitTimeCfgCommands = 1,

            .controllerMiscOption =
                (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable),
            .deviceType    = 0x1,
            .sflashPadType = kSerialFlash_4Pads,
            .serialClkFreq = kFlexSpiSerialClk_SDR_48MHz,
            .sflashA1Size  = 0x1000000,
            .sflashA2Size  = 0,
            .sflashB1Size  = 0,
            .sflashB2Size  = 0,
            .lookupTable =
                {
                    /* Read */
                    [0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
                    [1] = FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),

                    /* Read Status */
                    [4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x04),

                    /* Write Enable */
                    [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0x00),

                },
        },
    .pageSize           = 0x100,
    .sectorSize         = 0x1000,
    .ipcmdSerialClkFreq = 1,
    .blockSize          = 0x10000,
};
#endif /* BOOT_HEADER_ENABLE */

I am unsure if i need to modify the bootheader more, as this is just a copy of the example from Super Monkey, or if maybe I'm not using the correct driver for the QSPI? Any suggestions? 

Labels (1)
0 Kudos
Reply
7 Replies

2,081 Views
jay_heng
NXP Employee
NXP Employee

You need a unit test project to access this S25FL256. I will add RT600 target project in my RT-MFB

https://github.com/JayHeng/RT-MFB

1,956 Views
Hthornburgh
Contributor II
Hey Jay, would you be able to add the RT600 target project for MCUXpresso? We are still struggling with the initial bring-up. Thank you!
0 Kudos
Reply

2,057 Views
VCT
Contributor I
Hi Jay, I'm a colleague of Hthornburgh. Just realized that RT-MFB is currently an IAR project, after failing to import it in MCUXpresso yesterday.

Would you mind adding project files for MCUXpresso to RT-MFB repo?
0 Kudos
Reply

2,067 Views
Hthornburgh
Contributor II

Also is there any documentation anywhere that contains instructions for building with these tools?

0 Kudos
Reply

2,071 Views
Hthornburgh
Contributor II

Thank you, will you please let me know when you add the RT600 target project? I don't think I saw it in the link there.

0 Kudos
Reply

1,931 Views
jay_heng
NXP Employee
NXP Employee

Will add RT600 target this week.

2,083 Views
Hthornburgh
Contributor II

Here are some changes we've implemented in our bootheader. Can someone provide feedback on the questions within and advise if this looks like a bootheader issue or a driver issue?

/*
 * Copyright 2021 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */
#include "flash_config.h"

/* Hardware info:

  S25FL256SDPMFV001

  S25FL 256 S DP M F V 0 0 1
         |    |          |
        32MB 66MHz       |
                        uniform 64 kB sectors
  
  flash size = 32MB
  program buffer size = 512B
  erase sector size = 256kB
  erase block size = 32MB (whole device)

  t_css CS setup time = 3ns
  t_csh CS hold time = 3ns
*/

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.flash_config"
#endif

/*******************************************************************************
 * Code
 ******************************************************************************/
#if defined(BOOT_HEADER_ENABLE) && (BOOT_HEADER_ENABLE == 1)
#if defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".flash_conf"), used))
#elif defined(__ICCARM__)
#pragma location = ".flash_conf"
#endif

const flexspi_nor_config_t flexspi_config = {
    .memConfig =
        {
            .tag                  = FLASH_CONFIG_BLOCK_TAG,
            .version              = FLASH_CONFIG_BLOCK_VERSION,
            .csHoldTime           = 3,           // OK
            .csSetupTime          = 3,           // OK
            .configCmdEnable      = 0,
            .controllerMiscOption = (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable),
            .deviceType           = 0x1,         // FIXME!!! NOT SFDP COMPATIBLE, WHAT GOES HERE??
            .sflashPadType        = kSerialFlash_4Pads,          // OK
            .serialClkFreq        = kFlexSpiSerialClk_SDR_24MHz, // OK
            .sflashA1Size         = 0x2000000U,  // CHANGED
            .sflashA2Size         = 0,           // OK
            .sflashB1Size         = 0,           // CHANGED
            .sflashB2Size         = 0,           // OK
            .lookupTable =
                {
                    /* Read */
                                       // cmd0,    pad0,         op0,  cmd1,      pad1,         op1
                    [0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEC, RADDR_SDR, FLEXSPI_4PAD, 0x20), 
		                          // 1-bit-wide command value=0xEC
					  // 4-bit-wide read address length=32 bits
                    [1] = FLEXSPI_LUT_SEQ(MODE8_SDR, FLEXSPI_4PAD, 0x00, DUMMY_SDR, FLEXSPI_4PAD, 0x04),
		                          // 4-bit-wide mode value=0x0
					  // 4-bit-wide dummy for 4 clocks
                    //[2] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00),
                    [2] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 0x02, STOP_EXE, FLEXSPI_1PAD, 0x00),
					  // 4-bit-wide read data length=2 bytes
					  // NOP

                    /* Read Status */

		    //FIXME: what fields does the driver need from status register? Reg format is likely different

                    //[4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x04),
                                               // cmd0,    pad0,         op0,  cmd1,     pad1,         op1
                    [4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x01),
		                                  // 1-bit-wide command value=0x05
					          // 1-bit-wide read data length=1 byte

                    /* Write Enable */
                                               // cmd0,    pad0,         op0,  cmd1,     pad1,         op1
                    [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0x00),
		                                  // 1-bit-wide command value=0x06
					          // NOP

                    /* Sector erase */
                                               // cmd0,    pad0,         op0,  cmd1,      pad1,         op1
                    [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x21, RADDR_SDR, FLEXSPI_1PAD, 0x20),
		                                 // 1-bit-wide command value=0x21
					         // 1-bit-wide read address length=32 bits

                    /* block erase */
                                               // cmd0,    pad0,         op0,  cmd1,      pad1,         op1
                    [4 * 8 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xDC, RADDR_SDR, FLEXSPI_1PAD, 0x20),
		                                 // 1-bit-wide command value=0xdc
					         // 1-bit-wide read address length=32 bits

                    /* 4PP4B */
                    //[4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x3E, RADDR_SDR, FLEXSPI_4PAD, 0x20),
                    [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x34, RADDR_SDR, FLEXSPI_1PAD, 0x20),
		                                  // 1-bit-wide command value=0x34
					          // 1-bit-wide address length=32 bits
                    [4 * 9 + 1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_4PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00),
		                                  // 4-bit-wide write data length=0x4
					          // NOP

                    /* chip erase */
                    [4 * 11 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60, STOP_EXE, FLEXSPI_1PAD, 0x00),
		                                   // 1-bit-wide command value=0x60
					           // NOP
                },
        },
    .pageSize           = 0x200,     // CHANGED
    .sectorSize         = 0x10000,   // CHANGED
    .ipcmdSerialClkFreq = 1,         // OK (SPI controller setting, not flash)
    .blockSize          = 0x2000000  // CHANGED
};
#endif /* BOOT_HEADER_ENABLE */ 

 

0 Kudos
Reply