Are there any guidelines for multiple chained MIMXRT105x JTAG PCB layout and MCU-LINK-Pro settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any guidelines for multiple chained MIMXRT105x JTAG PCB layout and MCU-LINK-Pro settings

ソリューションへジャンプ
679件の閲覧回数
RidiculousRichard
Contributor II

We are looking to include multiple MIMXRT105x chips along with other devices in a 5 pin JTAG chain (TMS, TCK, TDI, TDO and nTRST).

We have found AN4826, AN12419 and the MCU-LINK-PRO UM11673-2940346 documents.

Are there any other application notes or other documentation that could contain useful guidelines and instructions for PCB layout and how to write an appropriate custom MCU-LINK-PRO connection scripts.

 

Thank you for your help,

Richard

0 件の賞賛
返信
1 解決策
608件の閲覧回数
RidiculousRichard
Contributor II

Thank you for you help Sam. +1

My take away is that there is no additional NXP documentation to find detailed NCU-LINK-Pro configuration comparable to e.g. Segger's more expensive debug probe and it's documentation; no worries and thank you once again.

 

Best regards,

Richard 

元の投稿で解決策を見る

4 返答(返信)
612件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @RidiculousRichard 

Thanks for your questions, it seems you want to know how to find dedicated documentaion about JTAG or MCU-LINK-pro for program or debug when you use MIMXRT105X, e.g useful guidelines and instructions for PCB layout. There are some comments from my side, please help clarify more if my understanding is wrong.

 

1. MIMXRT1050 EVKB Board Hardware User’s Guide to find JTAG connetor (J21 is a standard 20-pin/2.54 mm Box Header Connector for JTAG)

Sam_Gao_0-1717490334065.png

2. MIMXRT1050-EVK Design Resouces to download the schematics, layout files, and gerber files (including Silkscreen) for layout reference

3. AN4826 published by 2014 is still good guidelines for Schematic and PCB Layout, also please refer MCU-LINK-Pro User Manual to find more details, or other from MCU-LINK-Pro Documentation, it works well with our MCUXpresso or 3rd part IDE.

Sam_Gao_1-1717490780729.png

 

Have a nice day.

Sam

 

Hi @Masmiseim 

Thanks for your information and input.

Have a nice day,

Sam

 

 

 

 

 

609件の閲覧回数
RidiculousRichard
Contributor II

Thank you for you help Sam. +1

My take away is that there is no additional NXP documentation to find detailed NCU-LINK-Pro configuration comparable to e.g. Segger's more expensive debug probe and it's documentation; no worries and thank you once again.

 

Best regards,

Richard 

659件の閲覧回数
Masmiseim
Senior Contributor I

Hello,

We did this with the 1170. The whole thing was very unspectacular and runs without any problems. If you want to achieve good performance, you should just follow the usual layout rules.
Microchip has also created a nice summary on chaining: https://onlinedocs.microchip.com/pr/GUID-73C92233-8EC5-497C-92C3-D52ED257761E-en-US-1/index.html?GUI...

How you have to adapt the connect script depends on the development environment you are using. In principle, you only have to configure the bits before and after the device to be addressed, in each case for the instruction and data register.
Unfortunately, I cannot say how this works with MCUXpresso. We use Rowley Crossworks, which makes this very easy.

Regards

626件の閲覧回数
RidiculousRichard
Contributor II
Thank you for the link and good experience report. +1

I'm hoping someone who knows of MCUXpresso & MCU-LINK-Pro configuration documents will post some links to them.
0 件の賞賛
返信