Hi,
I want to evaluate some performance on cortax-m7 CPU, so I chose the 1170 board.
I installed the DSP form emcraft and from there I want to access DWT registers for performance monitor.
To do that, I need to modify the DEMCR registers. However, I cannot even access it
Below code gave me a segmentation fault.
How can I access the register then?
Thanks
#include "stdio.h"
#include "stdint.h"
int main() {
uint32_t a = (volatile uint32_t)0xE000EDFC;
return 0;
}
Thanks all for kindly reply and suggestions,
Re "2) You assign the variable 'a' the _value_ of 0xE000EDFC ? Why ?"
My code snippet got modified (auto formatting).
The one I try to show is
uint32_t a = *(volatile uint32_t *)0xE000EDFC;
I want to read/write the content of this register to enable DWT.
However, I got error
(gdb) p *(volatile uint32_t*)0xE000edfc
Cannot access memory at address 0xe000edfc
I tried to create a simple test case with @nickwallis 's implementation.
To do that, I copied some structure declaration and macros from
CMSIS/Core/Include/core_cm7.h
e.g.
typedef struct
{
__IOM uint32_t DHCSR; /*!< Offset: 0x000 (R/W) Debug Halting Control and Status Register */
__OM uint32_t DCRSR; /*!< Offset: 0x004 ( /W) Debug Core Register Selector Register */
__IOM uint32_t DCRDR; /*!< Offset: 0x008 (R/W) Debug Core Register Data Register */
__IOM uint32_t DEMCR; /*!< Offset: 0x00C (R/W) Debug Exception and Monitor Control Register */
} CoreDebug_Type;
But I still got the same issue on the statement
CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk; // enable trace for DWT features
The statement above tried to modify the content of address 0xE000EDFC, so this is the same error I got before.
I did this exploration on linux dsp from emcrafts and used their gcc toolchain. Would this makes a different?
What environment/work flow do you use to make it work?
Thanks
Sorry, there were two '*' being eaten when I try to copy the snippet around.
What I am trying to do is something like
https://mcuoneclipse.com/2017/01/30/cycle-counting-on-arm-cortex-m-with-dwt/
to read the DWT_CYCCNT register.
I followed their code and got segmentation fault.
And below is my test code to show that I cannot read the content of this DEMCR register.
I got segmentation fault from it.
#include "stdio.h"
#include "stdint.h"
int main() {
uint32_t a = *(volatile uint32_t *)0xE000EDFC;
return 0;
}
Please answer my question 1) above.
What do you mean with "segmentation fault"? where is it (precisely) detected?
My DWT implementation on a RT106x (which is also M7) is like this:
//-----------------------------------------------------------------------------
// DWT.c 20140212 CHG
//-----------------------------------------------------------------------------
#include "System.h"
#include "dwt.h"
#include "fsl_device_registers.h"
extern unsigned int SystemCoreClock;
//-----------------------------------------------------------------------------
// Return number of nSec that a number of cycles represent
// Takes CPU clock into account
//-----------------------------------------------------------------------------
unsigned int timeDWT(unsigned int cycles) {
float clk;
// Get CPU frequency
clk=SystemCoreClock;
return (1E09 * (1.0/clk) * (float)cycles);
}
//-----------------------------------------------------------------------------
// Enable cycle counter
//-----------------------------------------------------------------------------
void enableDWT(void) {
CoreDebug->DEMCR |= (1<<24);
DWT->CTRL = 1;
DWT->CYCCNT = 0;
}
//-----------------------------------------------------------------------------
// return current cycle counter (counts CPU cycles)
//-----------------------------------------------------------------------------
unsigned int readDWT(void) {
return DWT->CYCCNT;
}
I'm not certain it's essential to do this, but in my implementation I unlock access to the DWT registers, like this:
// measure time
CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk; // enable trace for DWT features
DWT->LAR = 0xc5acce55; // unlock access to DWT registers
DWT->CYCCNT = 0; // reset the cycle count value
DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk; // enable the cycle counter
// DO SOMETHING HERE .......
DWT->CTRL &= ~DWT_CTRL_CYCCNTENA_Msk; // disable the cycle counter
cycles = DWT->CYCCNT;