About imxrt1050 RAM BANK0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imxrt1050 RAM BANK0

1,495 Views
wangtiegang
Contributor II

Can RT1050 onchip RAM BANK0 be used as NVRAM if I add a Batterry with SNVS power ?

I read datasheet ,I find confilict between Datasheet and AN12085

The datasheet said can't, But appnote said can .

Labels (1)
0 Kudos
Reply
4 Replies

1,327 Views
igorpadykov
NXP Employee
NXP Employee

Hi 铁钢 王 

seems this is not possible based on Figure 45-1. Power system overview

i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Could you point where appnote said can.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,327 Views
wangtiegang
Contributor II

What  I  Think is  

Can I simply use a battery that can use the RTC and use RAM BANK0 as NVRAM?

Or I must use NVRAM external ?

0 Kudos
Reply

1,327 Views
wangtiegang
Contributor II

Table 8. Description of OCRAM bank

How to use iMXRT Low Power feature, Application Note, Rev. 0, 11/2017

pastedImage_1.png

According this table 

I think I can use Bank0 as NVRAM, if a battery is added

0 Kudos
Reply

1,327 Views
igorpadykov
NXP Employee
NXP Employee

below this app note, there is no such Table 8

AN12094 Power consumption and measurement of i.MXRT1050

https://www.nxp.com/docs/en/application-note/AN12094.pdf 

0 Kudos
Reply