hai,
I have been trying to interface a tft display with the imx6q sabreliteboard.I have already configured the board with yocto using core-image-x11.How can I install qt5 on it ?Can anybody provide the steps for that.Does the core-image-x11 support qt?Or should I bitbake it again with fsl-image-gui?
Thanks in advance
Hello,
NXP BSP contains configuration(s) to build "fsl-image-qt5".
Please refer to BSP documentation for more details.
https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&location=null
Also, the following may be helpful fsl-image-qt5 can support SABRE Lite ? how to config yocto bitbake?
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
when i tried fsl-image-qt5 i got error.What shoould I do now ? Does the image availabe to me (that is : bitbake core-image-x11) b not have qt support?