在使用yocto项目生成image过程中涉及到一些busybox中的命令行增加、删除,比如,我想删除busybox中的udhcpc的命令:
bitbake -c menuconfig busybox 去掉udhcpc的选项
bitbake busybox 重新编译busybox
bitbake core-image-base重新生成image,生成的image中仍然带udhcpc,我该如何修改busybox去掉或增加一些命令?是否需要修改bb文件中的SRC_URI?去掉ftp://xxxxxx/udhcpc
已解决! 转到解答。
Hi luo yaojun,
You can follow the below steps to disable just udhcpc from the image file:
1. $ bitbake -c menuconfig busybox
2. Unselect udhcpc and udhcpd.
Save & exit
3. $bitbake -c diffconfig busybox
4. Create busybox_%.bbapend under directory:
sources/poky/meta/recipes-core/busybox/
Add below two lines in the file created above:
FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://fragment.cfg
5. Copy the file (fragment.cfg) created in step 3 to sources/poky/meta/recipes-core/busybox/
Copy below to line to the file fragment.cfg
CONFIG_UDHCPD=n
CONFIG_UDHCPC=n
6. $bitbake <image>
You can see the sbin will not contain udhcpc.
Also, you can follow the below document for package dependencies and task list:
https://community.nxp.com/docs/DOC-94953
Regards,
Karan Gajjar
Hi luo yaojun,
Have you tried modifying conf/local.conf? You can follow the Yocto Project Reference Manual and check out the macros that we can use to remove the packages that we do need. Like PACKAGE_EXCLUDE, BAD_RECOMMENDATIONS.
Regards,
Karan Gajjar
Hi luo yaojun,
We checked with BAD_RECOMMENDATIONS = "busybox-udhcpc" in conf/local.conf. After rebuilding the image, we could not any file with *udhcpc* in the roots. Can you let us know if above command works? And which binary file you want to remove?
Regards,
Karan Gajjar
我想要删除image中的udhcpc命令,而这个命令是通过busybox生成的:
lrwxrwxrwx 1 root root 19 4月 6 07:53 sbin/udhcpc -> /bin/busybox.nosuid
这样的命令我该如何删除?
另外:
我该如何知道哪个命令属于那个package,例如:我需要添加useradd命令(非adduser命令,adduser是通过busybox生成的),这个命令应该是需要单独下载源码编译的,dot文件中没有找到useradd的相关信息,但是fsl-image-qt5这个image中包含了useradd命令。我该append哪个package来安装它们?
Hi luo yaojun,
You can add the following lines in your local.conf.
VIRTUAL-RUNTIME_base-utils = "" VIRTUAL-RUNTIME_login_manager = "shadow"
NOTE: This will remove all busybox commands from the image.
Do you want to remove all busybox commands or just udhcpc?
Regards,
Karan Gajjar
只想去掉udhcpc命令。
是否有相关文档描述在yocto中新增、删除某个命令或者库所需要的depend包名字?
例如我需要添加alsa库,我使用bitbake -s |grep alsa-*搜索结果如下:
alsa-lib :1.0.28-r0
alsa-lib-native :1.0.28-r0
alsa-oss :1.0.17-r1
alsa-state :0.2.0-r5
alsa-tools :1.0.28-r0
alsa-utils :1.0.28-r1
alsa-utils-alsaconf :1.0.28-r1
flite-alsa :1.3-r1
fsl-alsa-plugins :1.0.25-r0
nativesdk-alsa-lib :1.0.28-r0
python-pyalsaaudio :0.4-ml2
这些package各自包含哪些内容?是否有相关文档描述?
Hi luo yaojun,
You can follow the below steps to disable just udhcpc from the image file:
1. $ bitbake -c menuconfig busybox
2. Unselect udhcpc and udhcpd.
Save & exit
3. $bitbake -c diffconfig busybox
4. Create busybox_%.bbapend under directory:
sources/poky/meta/recipes-core/busybox/
Add below two lines in the file created above:
FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://fragment.cfg
5. Copy the file (fragment.cfg) created in step 3 to sources/poky/meta/recipes-core/busybox/
Copy below to line to the file fragment.cfg
CONFIG_UDHCPD=n
CONFIG_UDHCPC=n
6. $bitbake <image>
You can see the sbin will not contain udhcpc.
Also, you can follow the below document for package dependencies and task list:
https://community.nxp.com/docs/DOC-94953
Regards,
Karan Gajjar