您好:
太远了,您只要把wm8960的源码和移植步骤给我就行了,谢谢!
2015-01-16
石家庄开发区天远科技有限公司
开发一部 韩士龙
手机:15127185610
地址:石家庄市黄河大道227号
发件人:Lei Ge <admin@community.freescale.com>
发送时间:2015-01-16 11:12
主题:Re: - wm8960声卡驱动移植
收件人:"士龙 韩"<hanshilong622@163.com>
抄送:
wm8960声卡驱动移植
reply from Lei Ge in i.MX Community - View the full discussion
你能和FAE申请到我们公司来吗?你带设备来,我帮你一起调。
Did your question get answered?
If so, say thanks by clicking Correct Answer in the community thread!
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following wm8960声卡驱动移植 in these streams: Inbox
Hi 士龙
one can use WM8962 codec driver, since WM8962 is used on Sabre board
i.MX6_SABRE_SDP_DESIGNFILES : Design files (SPF-27392 p.10)
attached Linux Manual Table 23-1. Stereo Codec SoC Driver Files
shows driver files location
L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------