why when I mount mmc2 system is to mount mmc3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

why when I mount mmc2 system is to mount mmc3

939 次查看
tomgao
Contributor III

My command is :

imx6qsabresd login: root
root@imx6qsabresd:~# mmc2: host does not support reading read-only switch. assuming write-enable.
mmc2: new high speed SDHC card at address 1234
mmcblk2: mmc2:1234 SA32G 28.9 GiB
mmcblk2: p1

root@imx6qsabresd:~# mount -t vfat /dev/mmcblk2p1 sd
FAT-fs (mmcblk3p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
root@imx6qsabresd:~#

标签 (3)
0 项奖励
回复
1 回复

786 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tom

it may be useful to look at attached Linux Guide for emmc numbering rules,

sect.4.7.1 Running Linux OS from MMC/SD, Table 31. Linux uSDHC relationships

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复