why is linux i.mx6 uart dcedte setup in imx_set_termios

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

why is linux i.mx6 uart dcedte setup in imx_set_termios

2,640 次查看
andrewdyer
Contributor III

I am trying to set up the i.MX6 uart1 port as a DTE port to connect to a modem with full modem control.  Linux kernel is 3.10.17-1.0.2_ga.  I am seeing odd behaviour for the DCEDTE bit.

If I add the fsl,dte-mode property to my device tree, I see the property reflected in the kernel view of the device tree (/proc/device-tree/soc/aips-bus@02000000/spba-bus@02000000/serial@02020000/fsl,dte-mode file exists).  If I look at the UART1_UFCR register, the DCEDTE bit is not set.  At this no software has the port open (co console, no getty, no ppp, no autodialer).  When I check the IOMUXC all of the uart IO selected for uart1.

# /unit_tests/memtool UART1.UFCR

SOC: i.MX6DL

UART1    Addr:0x2020000

  UART1.UFCR Addr:0x02020090 Value:0x00000801 -

     UART1.UFCR.RXTL(0..5)      :0x1

             Receiver Trigger Level .

     UART1.UFCR.DCEDTE(6..6)    :0x0    <---------------------

             DCE/DTE mode select .

     UART1.UFCR.RFDIV(7..9)     :0x0

             Reference Frequency Divider.

     UART1.UFCR.TXTL(10..15)    :0x2

             Transmitter Trigger Level .

Digging in drivers/tty/serial/imx.c it looks like the DCEDTE bit is set in imx_set_termios().  As far as I can tell this function isn't called unless the port is opened. 

I think this is a bug - DCEDTE affects the IOMUX direction for all the port bits.  It seems to me that it should be set much earlier, preserved across the whole driver, and set regardless if the port is opened or not to minimize any IO contention.

标签 (3)
标记 (4)
0 项奖励
回复
4 回复数

1,899 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Andrew,

Could you prepare a patch (against kernel 3.19 or 4.0-rc7) and submit it to linux-serial mailing list for review and discuss?

Regards,

Fabio Estevam

0 项奖励
回复

1,899 次查看
andrewdyer
Contributor III

Unfortunately time constraints prevent me from doing this.  We reversed the connections on the uart on the PCB, abandoned using the additional flow control bits and use DCE mode now.

0 项奖励
回复

1,899 次查看
Yuri
NXP Employee
NXP Employee

  Basically it is the right approach to implement UART features  through

the Device Tree, in order to provide all the driver settings on the Device

Tree and avoid conflicts by setting the register manually outside it.

  Perhaps, You would need to modify the driver (and - maybe - add the
required feature to the Device Tree for selected UART port.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,899 次查看
andrewdyer
Contributor III

I'm not saying implementing the feature via device tree is wrong.  I think the implementation of the IO setup in the driver is in the wrong place and should happen as soon as possible.

0 项奖励
回复