which file i have to flash into sd card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which file i have to flash into sd card

233 Views
srinivas_123
Contributor III

I am using imx8mplus custom board . i build the SDK tool chain of 6.6 BSP.

i  build the uboot image . but which file i have to flash into sd card . could anyone please help me.
steps i followed to build the  uboot image.

git clone https://github.com/nxp-imx/uboot-imx -b lf_v2023.04
cd uboot-imx

make distclean
make imx8mp_evk_defconfig
make.

files after make :

u-boot-spl
u-boot-spl-nodtb.bin
u-boot-spl-dtb.bin
u-boot-spl.bin
u-boot-spl.sym
u-boot.img
u-boot-dtb.img
u-boot.elf

 

which file i have to consider as boot file and i have to flash into sd card.

Thanks&regards

srinivas

0 Kudos
Reply
1 Reply

212 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @srinivas_123!

 

Thank you for contacting NXP Support!

 

U-boot is only one part of the final binary to flash into our boards.

 

You can follow the chapter "4.5.13 How to build imx-boot image by using imx-mkimage"

 

In that chapter you can follow step by step how to generate the final binary to be flashed in your board.

 

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 

Best Regards!

Chavira

0 Kudos
Reply