where to get imx8mp airobot ap1302 camre fw

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where to get imx8mp airobot ap1302 camre fw

Jump to solution
894 Views
Nobita
Contributor III

Hello Sirs,

I am using imx8mp ai robot platform, and my code base is imx-yocto-bsp-5.10.72-2.2.3 refers to https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%... , howerver when I try to use the rpi-cam-mipi on it,it says it need fw ap1302_ar1355_1080p60_27M.binhowever I cannot found it on the repo https://github.com/ONSemiconductor/ap1302_binaries which is recommended by the rpi-cam-mipi doc, please tell me where to get the corresponding firmware of this camera sensor.

root@imx-robot-foxy:/lib/modules/5.10.72-lts-5.10.y+g26b899af4934/kernel/drivers/staging/media/imx# insmod imx_ap1302.ko
[   54.541920] imx_ap1302: module is from the staging directory, the quality is unknown, you have been warned.
[   54.552969] ap1302_mipi 1-003c: ap1302 probe called.
[   54.558605] Write pca957x error: val=0x1
[   54.564858] Write pca957x error: val=0x23
[   54.571489] Write pca957x error: val=0x33
[   54.577796] Write pca957x error: val=0x37
[   54.584389] Write pca957x error: val=0x3f
[   54.588688] Write pca957x error: val=0x1
[   54.592904] Write pca957x error: val=0xbf
[   54.630425] ap1302_mipi 1-003c: Direct firmware load for ap1302_ar1355_1080p60_27M.bin failed with error -2
[   54.640173] ap1302_mipi 1-003c: Falling back to sysfs fallback for: ap1302_ar1355_1080p60_27M.bin
[   54.649805] ap1302_mipi 1-003c: ap1302_request_firmware failed. ret=-2
[   54.656384] ap1302_mipi 1-003c: Cannot request ap1302 firmware.
[   54.664387] ap1302_mipi: probe of 1-003c failed with error -2

 

Thanks,Sincerely

0 Kudos
1 Solution
777 Views
Nobita
Contributor III

Sorry for that I forget to share my latest news, I use another bord, it works well!

Thanks!

View solution in original post

0 Kudos
5 Replies
266 Views
Nobita
Contributor III

Share my debug note and patches, hopes that can help other people.

0 Kudos
814 Views
Nobita
Contributor III

Finally, I have made the driver works, but I cannot preview the camera or record any YUV data to file, following are details:

  1. change my code base to 5.15.71-2.2.0 refers to https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B... , because this code base 's kernel version is 5.15.71 which has the same driver of ap1302 as imx93 does;
  2. patch the attached path of kernel, the patch is about the dts config for imx8mp-ai-robot platform;
  3. copy the imx93's ap1302.fw to the bord refers to https://docs.nxp.com/bundle/UM11933/page/topics/getting_started.html , I got the log says that the fw load success:

 

 

 

[    2.805324] ap1302_mipi 1-003c: AP1302 Chip ID is 0x265
[    2.810659] ap1302_mipi 1-003c: Direct firmware load for imx/camera/ap1302.fw failed with error -2
[    2.813112] ap1302_mipi 1-003c: AP1302 is found
[    2.819672] ap1302_mipi 1-003c: Falling back to sysfs fallback for: imx/camera/ap1302.fw
[    6.530390] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[    6.549580] mxc-md 32c00000.bus:camera: Entity type for entity ap1302_mipi 1-003c was not initialized!
[    6.560558] mx8-img-md: Registered sensor subdevice: ap1302_mipi 1-003c (1)
[    6.568136] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[    6.577608] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[    6.589038] mx8-img-md: created link [ap1302_mipi 1-003c] => [mxc-mipi-csi2.0]
[   24.478006] ap1302_mipi 1-003c: Load firmware successfully.​

 

 

 

    4. use the comand to preview or record YUV data fo file refers to https://docs.nxp.com/bundle/UM11933/page/topics/software_introduction.html , unfortunately it got nothing, no preview on my HDMI monitor, the record file size is 0, here is the terminal log when do preview

 

 

 

root@imx-robot-foxy:~# gst-launch-1.0 -v v4l2src device=/dev/video3 ! "video/x-raw,format=YUY2,width=1280,height=800" ! queue ! waylandsink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipelin[   57.387455] bypass csc
e0/GstV4l2Src:v4l2src0.GstPad:src[   57.392240] input fmt YUV4
: caps = video/x-raw, format=(str[   57.397812] output fmt YUYV
ing)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1


[ 1018.967454] audit: type=1006 audit(1651206601.900:4): pid=1459 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[ 1018.979853] audit: type=1300 audit(1651206601.900:4): arch=c00000b7 syscall=64 success=yes exit=1 a0=3 a1=ffffe9948370 a2=1 a3=ffff90756020 items=0 ppid=416 pid=1459 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="crond" exe="/usr/sbin/crond" key=(null)
[ 1019.005595] audit: type=1327 audit(1651206601.900:4): proctitle=2F7573722F7362696E2F63726F6E64002D6E


^Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:20:14.988214000
Setting pipeline to NULL ...
Freeing pipeline ...
​

 

 

 

    5.I check the voltage test points on RPI-CAM-MIPI board, the voltages are correct.

Please give me some advice to inspect the issue.

Thanks in advance.

0 Kudos
783 Views
joanxie
NXP TechSupport
NXP TechSupport

do you have imx8mp evk board or 93evk board? I don't have airobot board to test this, but verified on imx8mp evk board, I don't know if this code can work on airobot board or not

0 Kudos
778 Views
Nobita
Contributor III

Sorry for that I forget to share my latest news, I use another bord, it works well!

Thanks!

0 Kudos