where is the driver of tvp5158 connect to IMX6Q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is the driver of tvp5158 connect to IMX6Q?

810 Views
翔李
Contributor IV

hi,

  I use tvp5158(TI) to capture 4 D1 camera to connect to imx6q throgh csi0_data[19:12] and pixclk,but it is not capture video information.

So,can you give me the driver code of tvp5158-imx6q?

Following is link of tvp5158,

www.ti.com.cn/product/cn/tvp5158

Thanks.

Labels (4)
0 Kudos
Reply
2 Replies

574 Views
igorpadykov
NXP Employee
NXP Employee

Hi

there is no driver for it in BSPs provided by NXP, as it can not be supported directly,

that is i.MX6 can capture the combined video into memory, but software

should split it to four videoes. Seems some customers succeeded as

using TV decoder(tvp5158) on IMX6

https://community.nxp.com/message/358505#comment-358505

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

574 Views
翔李
Contributor IV

Thanks a lot.

There is no reply after I asking for tvp5158 driver code on imx6.so can you help me to do it,for my weak english skill.my email address is xiang.li@ivicar.cn

Thank you,boss.

0 Kudos
Reply