You want to know the boot flag or container flag?
If it is container flag, it is in the reference manual and as you have already shown them.
and it is about the authentication. not for the imx-mkimage "-flag". It is used by the code-signing tool.
If it is boot flag.
Please refer to System Controller Firmware Porting Guide
Hi ZHOUNENG
for imx-mkimage flags one can look at imx-mkimage documentation
https://source.codeaurora.org/external/imx/imx-mkimage/tree/README?h=lf-5.10.y_2.0.0
Best regards
igor
Hello igor
Thanks for help, I can get only the following information from the README file of imx-mkimage git repo.
-flags [value] Specifies flags for the new container. The value needs to be a 32bit value in hex.
You want to know the boot flag or container flag?
If it is container flag, it is in the reference manual and as you have already shown them.
and it is about the authentication. not for the imx-mkimage "-flag". It is used by the code-signing tool.
If it is boot flag.
Please refer to System Controller Firmware Porting Guide