what is imx8 core base for jtag ~~Help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

what is imx8 core base for jtag ~~Help

跳至解决方案
5,809 次查看
fatalfeel
Contributor V

for jtag openocd

I get BSDL file for i.MX 8M (REV 1)  

it's 0x1cf80553 for sjc_tapid

# System JTAG Controller
if { [info exists SJC_TAPID] } {
        set _SJC_TAPID $SJC_TAPID
} else {
        set _SJC_TAPID 0x1cf80553
}
set _SJC_TAPID2 0x2cf80553

jtag newtap $_CHIPNAME sjc -irlen 5 -ircapture 0x01 -irmask 0x1f \
        -expected-id $_SJC_TAPID -expected-id $_SJC_TAPID2

now i.mx8

1. need Base addresses of cores

2. CoreSight Debug Access Port

 

///////////////////////////////////////////////////////////////////////

this is for arm arch64

///////////////////////////////////////////////////////////////////////

set _cores 8
for { set _core 0 } { $_core < $_cores } { incr _core 1 } {

    set _command "target create ${_TARGETNAME}$_core aarch64 \
                         -chain-position $_CHIPNAME.dap -coreid $_core -ctibase [set $_TARGETNAME.cti($_core)]"

    if { $_core != 0 } {
        # non-boot core examination may fail
        set _command "$_command -defer-examine"
        set _smp_command "$_smp_command ${_TARGETNAME}$_core"
    } else {
        # uncomment when "hawt" rtos is merged
        # set _command "$_command -rtos hawt"
        set _smp_command "target smp ${_TARGETNAME}$_core"
    }

    eval $_command
}

eval $_smp_command

# declare the auxiliary Cortex-M3 core on AP #2 (runs mcuimage.bin)
target create ${_TARGETNAME}.m3 cortex_m -chain-position $_CHIPNAME.dap -ap-num 2 -defer-examine

///////////////////follow is for imx.6 info ///////////////////

# CoreSight Debug Access Port
if { [info exists DAP_TAPID] } {
        set _DAP_TAPID $DAP_TAPID
} else {
        set _DAP_TAPID 0x4ba00477
}

jtag newtap $_CHIPNAME dap -irlen 4 -ircapture 0x01 -irmask 0x0f \
        -expected-id $_DAP_TAPID

# SDMA / no IDCODE
jtag newtap $_CHIPNAME sdma -irlen 4 -ircapture 0x00 -irmask 0x0f

# System JTAG Controller
if { [info exists SJC_TAPID] } {
        set _SJC_TAPID $SJC_TAPID
} else {
        set _SJC_TAPID 0x0191c01d
}
set _SJC_TAPID2 0x0191e01d
set _SJC_TAPID3 0x2191c01d
set _SJC_TAPID4 0x2191e01d

jtag newtap $_CHIPNAME sjc -irlen 5 -ircapture 0x01 -irmask 0x1f \
        -expected-id $_SJC_TAPID -expected-id $_SJC_TAPID2 \
        -expected-id $_SJC_TAPID3 -expected-id $_SJC_TAPID4

# GDB target: Cortex-A9, using DAP, configuring only one core
# Base addresses of cores:
# core 0  -  0x82150000
# core 1  -  0x82152000
# core 2  -  0x82154000
# core 3  -  0x82156000
set _TARGETNAME $_CHIPNAME.cpu.0
target create $_TARGETNAME cortex_a -chain-position $_CHIPNAME.dap \
        -coreid 0 -dbgbase 0x82150000

标记 (1)
0 项奖励
1 解答
4,009 次查看
fatalfeel
Contributor V

# Freescale i.MX8 series single/dual/quad core processor

if { [info exists CHIPNAME] } {
   set  _CHIPNAME $CHIPNAME
} else {
   set  _CHIPNAME imx8
}

# Debug Access Port
if { [info exists DAP_TAPID] } {
        set _DAP_TAPID $DAP_TAPID
} else {
        set _DAP_TAPID 0x5ba00477
}

jtag newtap $_CHIPNAME dap -irlen 4 -ircapture 0x01 -irmask 0x0f \
        -expected-id $_DAP_TAPID

# SDMA / no IDCODE
#jtag newtap $_CHIPNAME sdma -irlen 4 -ircapture 0x00 -irmask 0x0f

# SOC JTAG ID / IDCODE refer to BSDL file
#if { [info exists SJC_TAPID] } {
#        set _SJC_TAPID $SJC_TAPID
#} else {
#        set _SJC_TAPID 0x1cf80553
#}
#set _SJC_TAPID1 0x2cf80553

#jtag newtap $_CHIPNAME sjc -irlen 5 -ircapture 0x01 -irmask 0x1f \
        -expected-id $_SJC_TAPID -expected-id $_SJC_TAPID1

# GDB target: Cortex-A53, using DAP, configuring only one core
# Coresight base address:
# core 0  -  0x80410000 / cti - 0x80420000
# core 1  -  0x80510000 / cti - 0x80520000
# core 2  -  0x80610000 / cti - 0x80620000
# core 3  -  0x80710000 / cti - 0x80720000
set _TARGETNAME $_CHIPNAME.cpu0
#set _TARGETNAME_1 $_CHIPNAME.cpu1
#set _TARGETNAME_2 $_CHIPNAME.cpu2
#set _TARGETNAME_3 $_CHIPNAME.cpu3

target create $_TARGETNAME aarch64 -chain-position $_CHIPNAME.dap -coreid 0 -dbgbase 0x80410000 -ctibase 0x80420000
#target create $_TARGETNAME_1 aarch64 -chain-position $_CHIPNAME.dap -coreid 1 -dbgbase 0x80510000 -ctibase 0x80520000
#target create $_TARGETNAME_2 aarch64 -chain-position $_CHIPNAME.dap -coreid 2 -dbgbase 0x80610000 -ctibase 0x80620000
#target create $_TARGETNAME_3 aarch64 -chain-position $_CHIPNAME.dap -coreid 3 -dbgbase 0x80710000 -ctibase 0x80720000
        
# some TCK cycles are required to activate the DEBUG power domain
#jtag configure $_CHIPNAME.sjc -event post-reset "runtest 100"

proc imx8_dbginit {target} {
        # General Cortex-A53 debug initialisation
        aarch64 dbginit
}

# Slow speed to be sure it will work
adapter_khz 1000
$_TARGETNAME configure -event reset-start { adapter_khz 1000 }

$_TARGETNAME configure -event reset-assert-post "imx8_dbginit $_TARGETNAME"
$_TARGETNAME configure -event gdb-attach { halt }

在原帖中查看解决方案

0 项奖励
11 回复数
4,010 次查看
fatalfeel
Contributor V
0 项奖励
4,010 次查看
ranjith_tc
Contributor I

Hi Jesse stone,

Do you know the coresight base address for iMX8QMax(4 x A53+2 x A72)?

0 项奖励
4,010 次查看
fatalfeel
Contributor V

maybe same as imx8

need try ex:  like
# core 0  -  0x80A10000 / cti - 0x80A420000

 

0 项奖励
4,010 次查看
ranjith_tc
Contributor I

Okay. Thanks. Let me try that.

But I got reply from NXP support team that for this processor, the access to debug components is via a secure module.

So, do you know, how to do that?

0 项奖励
4,010 次查看
fatalfeel
Contributor V

jtag openocd eclipse

see the imx8m.cfg setting will give you answer
ver 0.10.1 test compile ok on ubuntu 16.04 x64
made on march 2020
http://fatalfeel.blogspot.com/2015/12/openocd-with-eclipse-debug-kernel-of.html

0 项奖励
4,010 次查看
fatalfeel
Contributor V

# Freescale i.MX8 series single/dual/quad core processor

if { [info exists CHIPNAME] } {
   set  _CHIPNAME $CHIPNAME
} else {
   set  _CHIPNAME imx8
}

# Debug Access Port
if { [info exists DAP_TAPID] } {
        set _DAP_TAPID $DAP_TAPID
} else {
        set _DAP_TAPID 0x5ba00477
}

jtag newtap $_CHIPNAME dap -irlen 4 -ircapture 0x01 -irmask 0x0f \
        -expected-id $_DAP_TAPID

# SDMA / no IDCODE
#jtag newtap $_CHIPNAME sdma -irlen 4 -ircapture 0x00 -irmask 0x0f

# SOC JTAG ID / IDCODE refer to BSDL file
#if { [info exists SJC_TAPID] } {
#        set _SJC_TAPID $SJC_TAPID
#} else {
#        set _SJC_TAPID 0x1cf80553
#}
#set _SJC_TAPID1 0x2cf80553

#jtag newtap $_CHIPNAME sjc -irlen 5 -ircapture 0x01 -irmask 0x1f \
        -expected-id $_SJC_TAPID -expected-id $_SJC_TAPID1

# GDB target: Cortex-A53, using DAP, configuring only one core
# Coresight base address:
# core 0  -  0x80410000 / cti - 0x80420000
# core 1  -  0x80510000 / cti - 0x80520000
# core 2  -  0x80610000 / cti - 0x80620000
# core 3  -  0x80710000 / cti - 0x80720000
set _TARGETNAME $_CHIPNAME.cpu0
#set _TARGETNAME_1 $_CHIPNAME.cpu1
#set _TARGETNAME_2 $_CHIPNAME.cpu2
#set _TARGETNAME_3 $_CHIPNAME.cpu3

target create $_TARGETNAME aarch64 -chain-position $_CHIPNAME.dap -coreid 0 -dbgbase 0x80410000 -ctibase 0x80420000
#target create $_TARGETNAME_1 aarch64 -chain-position $_CHIPNAME.dap -coreid 1 -dbgbase 0x80510000 -ctibase 0x80520000
#target create $_TARGETNAME_2 aarch64 -chain-position $_CHIPNAME.dap -coreid 2 -dbgbase 0x80610000 -ctibase 0x80620000
#target create $_TARGETNAME_3 aarch64 -chain-position $_CHIPNAME.dap -coreid 3 -dbgbase 0x80710000 -ctibase 0x80720000
        
# some TCK cycles are required to activate the DEBUG power domain
#jtag configure $_CHIPNAME.sjc -event post-reset "runtest 100"

proc imx8_dbginit {target} {
        # General Cortex-A53 debug initialisation
        aarch64 dbginit
}

# Slow speed to be sure it will work
adapter_khz 1000
$_TARGETNAME configure -event reset-start { adapter_khz 1000 }

$_TARGETNAME configure -event reset-assert-post "imx8_dbginit $_TARGETNAME"
$_TARGETNAME configure -event gdb-attach { halt }

0 项奖励
4,010 次查看
fatalfeel
Contributor V

openocd 2018 03 01 merge and update jaylink deiver

search key word ->  openocd-0.10.0_v13.tar.gz  and download

http://fatalfeel.blogspot.tw/2015/12/openocd-with-eclipse-debug-kernel-of.html


./configure --prefix=/opt/openocd --enable-maintainer-mode --enable-ftdi --enable-target64
make && make install

find -> imx8.cfg  //done

0 项奖励
4,010 次查看
fatalfeel
Contributor V
0 项奖励
4,010 次查看
diegoadrian
NXP Employee
NXP Employee

I apologize for the delay.

But, what is exactly your question?

Best Regards,

Diego.

0 项奖励
4,010 次查看
fatalfeel
Contributor V

1. Base addresses of cores of imx8

2. CoreSight Debug Access Port of imx8

///////////////////////

ex:

base address of core of imx6 is 0x82150000

CoreSight Debug Access Port of imx6 is 0x4ba00477

0 项奖励
4,010 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Everything related to the cortex you can see it in the ARM documentation. For example, you can see on the below link the reference manual for the ARM cortex A-53, there are located the base address of the cortex.

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0500d/DDI0500D_cortex_a53_r0p2_trm.pdf 

I hope this can help you,

Best Regards,

Diego.

0 项奖励