uuu imx android flash does not work on imx7ulp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uuu imx android flash does not work on imx7ulp

936 次查看
zbigniewmazur
Contributor II

Andorid p9 BSP for imx processors using the new flasher tool on imx7ulp board gives this:

sudo ./uuu_imx_android_flash.sh -f imx7ulp -m -e


imx7ulp-evk does not support emmc as target device, change target device automatically

then the flashing stops forever. What should I do ?

Thank you!

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

746 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please check that the boot switches are in download mode,

sw1 (boot mode) to 01xx (from 1-4 bit) to enter download mode

 

Hope this helps,

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复