uuu: an in-depth description for script commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uuu: an in-depth description for script commands

1,807件の閲覧回数
IgorKorolyuk
Contributor I

Hello.

I'll have to bring up an iMX.8MDualCore based board soon, so I've been investigating tools to do that and discovered the UUU manual (UUU.pdf) to be quite poor on what those script command actually do. There are lots of user manual of how to run uuu to get a certain reference board flashed in a number of ways, but I've seen none describing uuu script commands in technincal details. ("SDPV: write -f _flash.bin -skipspl -scanterm" : what are all the options here? what is _flash.bin file format is expected to be?)

Is there an in-depth technical description for those commands? If there is, where can I get one?

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

867件の閲覧回数
harold_vanderpo
Contributor I

Here is a link to a doc that does provide some detail on the individual commands of each protocol in the uuu script.  https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.4.165/UUU.pdf

There is also another forum topic that provided this link and might be useful for those writing custom script https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Creating-and-running-a-custom-script-for...

 

0 件の賞賛
返信

1,799件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

_flash.bin stands for uboot bin file, you can replace this name to your own uboot bin file name

0 件の賞賛
返信

1,791件の閲覧回数
IgorKorolyuk
Contributor I

joanxie,

Thanks for the tip on this particular example but it's not full enough.

  • What are those two other command options?
  • The command is "write", right? Ok. What's the destination address? How does the uuu figure that out?

See, this sort of questions arise on all of the commands in script file, not just this particular one. That's why I'm asking for in-depth description on all of them.

0 件の賞賛
返信

1,779件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I don't know what you mean, you can find example uuu script file like "example_kernel_emmc.uuu" which is attached in the demo images,you can just replace your own image name

you also can refer to detailed source code and readme:

https://github.com/NXPmicro/mfgtools/blob/master/uuu/uuu.lst

https://github.com/NXPmicro/mfgtools

 

 

 

 

0 件の賞賛
返信

1,775件の閲覧回数
IgorKorolyuk
Contributor I

Thanks for the pointers

0 件の賞賛
返信