Hi NXP,
I am trying to flash Linux 5.15.52_2.1.0 to my i.MX 8QXP board 128G emmc, but got really slow speed as video.()
But if I use
L5.10.35_2.0.0_MX8QXPC0 > imx-boot-imx8qxpc0mek-sd.bin-flash_spl
With 5.15.52
imx-image-full-imx8qxpc0mek.wic
I can get normal flashing speed(Should be done in 10 min).
Can I change some config to make it faster?
Since the Flashing program will stop at " Flashing Sparse Image " as the video show
I notice that Flashing spends a lot of time in
uboot > lib/image-sparse.c > write_sparse_image > write_sparse_chunk_raw > while loop
Is any way I can reduce it?